Validation button
The validation button is used to verify the system has been configured correctly. If there are any problems with the system library, the library can be saved but it will not be available to select in the project.
Clicking the validation button will bring up a flyout pane that lists any problems with the system. If the problem relates to a specific component, click on the magnifying glass to highlight the component in the diagram.