Zone Level Equipment

 
If there are any zone level equipment included in the system, they will be listed in the Zone Level Equipment tab.  As pieces of equipment are added or removed, the list in the tab will update.  The equipment libraries can be selected here.
 
Component Name
This is the name of the specific component in the system and will match the tag name above the component in the system diagram.  This name is editable. 
 
Category
This is the library where this specific component is found. 
 
Type
This is a subcategory in the library where this specific component is found.
 
Library Items
This is the actual library member that will be used to represent this component.