Trace 3D Plus
User Guide
 
×

Utilization Schedules

 
Utilization schedules designate the percentage of a peak value that should be applied throughout the year. There are thirteen sub-types:
 
Each sub-type will be displayed in its applicable section of the project. For example, schedules created under the People sub-type will be displayed in the Internal Loads tab of the Room Properties and in the Internal Loads template.
 
 
Adjacent Zone Airflow Utilization Schedules
These schedules are displayed in the Create Building sub-section under the Airflow tab/Airflow transfer section of the Room Properties. It will define the percentage of the room airflow that can be transferred. The default values for the day profile graph are:
Timestep: 1
Grid Interval: 5
Y Precision: 0
Y Min: 0
Y Max: 100
Y Units: %
X Min: 12:00 AM
X Max: 11:59 PM
X Units: time
 
 
 
Between Glass Airflow Utilization Schedules
These schedules are displayed under Exterior Windows and Glass Doors. It defines the percent of the maximum between glass airflow that should be flowing at a certain time of the year.
Timestep: 1
Grid Interval: 5
Y Precision: 0
Y Min: 0
Y Max: 100
Y Units: %
X Min: 12:00 AM
X Max: 11:59 PM
X Units: time
 
 
Equipment Operation Utilization Schedules
These schedules are displayed Systems section under the Configure Zone Equipment subsection when a Radiant Heat or Wall Convector zone equipment is added to a zone. They are used for radiant skin equipment that is controlled based on OA temperature.
Timestep: 1
Grid Interval: 5
Y Precision: 0
Y Min: 0
Y Max: 100
Y Units: %
X Min: 12:00 AM
X Max: 11:59 PM
X Units: time
 
 
 
Exhaust Utilization Schedules
These schedules are displayed in the Create Building sub-section under the Airflow tab/Room Exhaust section of the Room Properties. It defines the percent of the maximum exhaust flow rate that should be applied at different times of the year.
Timestep: 1
Grid Interval: 5
Y Precision: 0
Y Min: 0
Y Max: 100
Y Units: %
X Min: 12:00 AM
X Max: 11:59 PM
X Units: time
 
 
Infiltration Utilization Schedules
These schedules are displayed in the Create Building sub-section under the Airflow tab/Infiltration section of the Room Properties. It defines the percent of the maximum infiltration flow rate that should be applied at different times of the year.
Timestep: 1
Grid Interval: 5
Y Precision: 0
Y Min: 0
Y Max: 100
Y Units: %
X Min: 12:00 AM
X Max: 11:59 PM
X Units: time
 
 
 
Lights Utilization Schedules
These schedules are displayed in the Create Building sub-section under the Internal Loads tab of the Room Properties and in the Internal Loads template. It defines the percent of the maximum light density that should be applied at different times of the year.
Timestep: 1
Grid Interval: 5
Y Precision: 0
Y Min: 0
Y Max: 100
Y Units: %
X Min: 12:00 AM
X Max: 11:59 PM
X Units: time
 
 
Miscellaneous Loads and Utilities Utilization Schedules
These schedules are displayed in the Create Building sub-section under the Internal Loads tab of the Room Properties and in the Internal Loads template. It defines the percent of the maximum miscellaneous load or miscellaneous utility density that should be applied at different times of the year.
Timestep: 1
Grid Interval: 5
Y Precision: 0
Y Min: 0
Y Max: 100
Y Units: %
X Min: 12:00 AM
X Max: 11:59 PM
X Units: time
 
 
 
Multipliers Utilization Schedules
These schedules are displayed in the Configure Plants sub-section under the Components tab of the Loop Properties when a District Cooling or District Heating component has been added to the loop. It is also used in the Plants section under the Demand Loads tab of the Loop Properties. In either case, the schedule defines the percent of the maximum peak load or capacity that should be applied at different times of the year.
Timestep: 1
Grid Interval: 5
Y Precision: 0
Y Min: 0
Y Max: 100
Y Units: %
X Min: 12:00 AM
X Max: 11:59 PM
X Units: time
 
 
People Utilization Schedules
These schedules are displayed in the Create Building sub-section under the Internal Loads tab of the Room Properties and in the Internal Loads template. It defines the percent of the maximum People density that should be applied at different times of the year.
Timestep: 1
Grid Interval: 5
Y Precision: 0
Y Min: 0
Y Max: 100
Y Units: %
X Min: 12:00 AM
X Max: 11:59 PM
X Units: time
 
 
 
Site Equipment Utilization Schedules
These schedules are displayed in the Create Site sub-section under the Power-Using Objects toolbar. It defines the percent of the maximum power that should be applied at different times of the year.
Timestep: 1
Grid Interval: 5
Y Precision: 0
Y Min: 0
Y Max: 100
Y Units: %
X Min: 12:00 AM
X Max: 11:59 PM
X Units: time
 
 
VAV Minimum Utilization Schedules
These schedules are displayed in the Configure Zone Equipment sub-section under the Terminal Device tab of the System properties. It defines the percentage of the defined or calculated system air flow that should be applied at different times of the year.
Timestep: 1
Grid Interval: 5
Y Precision: 0
Y Min: 0
Y Max: 100
Y Units: %
X Min: 12:00 AM
X Max: 11:59 PM
X Units: time
 
 
 
Ventilation Utilization Schedules
These schedules are displayed in the Create Building sub-section under the Airflow tab/Ventilation section of the Room Properties. It defines the percent of the maximum ventilation flow rate that should be applied at different times of the year.
Timestep: 1
Grid Interval: 5
Y Precision: 0
Y Min: 0
Y Max: 100
Y Units: %
X Min: 12:00 AM
X Max: 11:59 PM
X Units: time
 
 
Water Heater Flow Rates Utilization Schedules
These schedules are displayed in the Configure Plants sub-section under the Components tab of the Loop Properties when a Stratified or Mixed Water Heater component has been added to the loop. The schedule defines the percent of the peak flow rate that should be applied at different times of the year.
Timestep: 1
Grid Interval: 5
Y Precision: 0
Y Min: 0
Y Max: 100
Y Units: %
X Min: 12:00 AM
X Max: 11:59 PM
X Units: time